Call Toll Free 1-866-727-8376
Items in cart: (0) Cart Total: 0.00 USD

 

Pasternack’s New 3-Port Field Calibration Tools
 

With Pasternack’s new 3-Port Calibration Tools, engineers and installers in the field can make error-corrected measurements of devices supplied with 3.5mm, N-Type, or 7/16 DIN connectors. 3-Port Calibration Tools

 

Also called “Bones”, these tools are very effective when needing to make field calibrations as they are lightweight and portable. For this same reason, they can support in-house calibration requirements without the expense of Calibration Kits that can cost thousands of dollars. All models are fully compatible with a wide range of handheld Cable and Antenna Analyzers including the Anritsu SiteMaster™.  Each tool has either Male (Plug) or Female (Jack) connector interfaces to perform Short, Open, and Load measurements on the device you are evaluating. Fully RoHS and REACH Compliant. 

 

Pasternack’s 3-fort field calibration tools are stocked at the factory to support same-day shipment, with real-time pricing and inventory stock available online at www.pasternack.com.  Pricing is as low as $595.00 (US) for Type-N MALE connector tool.  For additional support, contact Pasternack toll-free by phone at (866) 727-8376 or by email at sales@pasternack.com.

 

 

For further information and reader enquiries:

 

Jake Ring, VP Sales & Marketing, Pasternack Enterprises,

 

Tel:      (949) 261-1920 x 120                   Email:   jake@pasternack.com

Fax:      (949) 261-7451                           Web:    www.pasternack.com

 

 

Note to editors:

 

Pasternack Enterprises started in 1972 in Irvine, California as a manufacturer of log amplifiers for the military and aerospace communities. Over the following 35 years Pasternack has evolved to offer one of the most extensive lines of RF coaxial and fiber optic products in the industry. In addition, the company provides value-added RF/Microwave and Fiber Optic cable assemblies, with custom and standard configurations available for same-day shipping. With the industry’s largest off-the-shelf inventory available for immediate delivery, Pasternack has become The Reliable Source for customers within multiple markets, including the telecommunications, instrumentation, military, consumer electronics, transportation, industrial equipment and medical equipment markets.