Call Toll Free 1-866-727-8376
Items in cart: (0) Cart Total: 0.00 USD

 

Pasternack Introduces New VNA Test Cable Kit
 

New VNA Test Cable Kit from Pasternack Enterprises

New VNA Test Cable Kit from Pasternack

The reliability and flexibility of Pasternack's PE310-KIT offers excellent electrical characteristics with outstanding phase and amplitude stability for use with Vector Network Analyzers (VNA). The PE310-KIT has unique interchangeable connector heads to allow fast and easy configuration for DUT Applications that require Precision 7mm (PC-7), N-type, 3.5mm, SMA or 2.92mm connections and operation from DC to 26.5GHz. The kit contains one pair of test cables packed in a durable, protective wood box.

Pasternack PE310-KIT is stocked at the factory to support same day shipment. Pricing is $3,499.95 for single piece delivery. Use Pasternack's on-line selection guide for complete specifications or to buy online at www.pasternack.com. For additional support, contact Pasternack by phone at (866) 727-8376 or by email at sales@pasternack.com.

For further information and reader enquiries:

 

Jake Ring, VP Sales & Marketing, Pasternack Enterprises,

 

Tel:      (949) 261-1920 x 120                   Email:   jake@pasternack.com

Fax:      (949) 261-7451                           Web:    www.pasternack.com

  

Note to editors:

 

Pasternack Enterprises started in 1972 in Irvine, California as a manufacturer of log amplifiers for the military and aerospace communities. Over the following 35 years Pasternack has evolved to offer one of the most extensive lines of RF coaxial and fiber optic products in the industry. In addition, the company provides value-added RF/Microwave and Fiber Optic cable assemblies, with custom and standard configurations also available for same-day shipping. With the industry’s largest off-the-shelf inventory available for immediate delivery, Pasternack has become The Reliable Source for customers within multiple markets, including the telecommunications, instrumentation, military, consumer electronics, transportation, industrial equipment and medical equipment markets.