Pasternack Blog

  • Categories

  • Archive

  • Why would you want to limit an amplifier?

    06/28/2018

    Amplifiers are electronic devices that increase the power of a signal. The amount of amplification in an amplifier is measured by its gain, or the ratio of output voltage, current, or power to the input with a power gain greater than one. An RF amplifier is similar to an audio amplifier but with components suitable ..

    Read Full Article

    Bits on Baluns – Part 3

    06/21/2018

    Basic Baluns The type of balun used in microwave RF designs depends on the bandwidth required, the operating frequency, and the physical architecture of the design. As differential power dividers, baluns can be transformers, capacitively and/or magnetically coupled transmission lines, hybrid couplers, or used in a combination of power divider and inverter. Baluns are used ..

    Read Full Article

    Bits on Baluns – Part 2

    06/14/2018

    Balun Performance Metrics There are many different types of baluns and the type of balun used in microwave RF designs depends on the bandwidth required, the operating frequency, and the physical architecture of the design. Most baluns usually contain two or more insulated copper wires twisted together and wound around or inside a core, magnetic ..

    Read Full Article

    Bits on Baluns

    06/07/2018

    Part 1: What is a balun, what does a balun do, and when is a balun needed? What is a balun? A balun (mashup of balanced and unbalanced) is a three-port device, or a type of broadband RF transmission line transformer, with a matched input and differential output that is used to connect balanced transmission ..

    Read Full Article
    Jump to of 1