IoT Network Types, Protocols, and Wireless Standards Blog Series (Part 3)

  • Categories

  • Archive

  • There are a multitude of layers, protocols, and wireless standards for IoT applications. The following blog gives a brief description of these layers and lists (with links!) to a variety of the leading protocols and standards relevant for IoT applications.

    IoT Application Protocols

    The Application layer protocols are typically responsible for data formatting and presentation, and are commonly based on the HTTP protocol. As HTTP may not be ideal for resource constrained applications, such as many IoT applications, many alternate application layer protocols have emerged.

    MQTT *Message Queue Telemetry Transport
    SMQTT *Secure MQTT
    CoAP *Constrained Application Protocol
    DDS *Data Distribution Service
    XMPP *Extensible Messaging and Presence Protocol
    AMQP *Advanced Message Queuing Protocol
    REST *Representational State Transfer
    MQTT-SN *MQTT for Sensor Networks
    STOMP *Simple Text Oriented Messaging Protocol
    SCMP *Simple Message Commerce Protocol
    SNMP *Simple Network Management Protocol
    LLAP *Lightweight Local Automation Protocol
    SSI *Simple Sensor Interface
    LWM2M *Lightweight M2M
    M3DA *Mihini
    XMPP-IOT *
    ONS 2.0 *Object Name Service
    SOAP *Simple Object Access Protocol
    Websocket
    Reactive Streams
    HTTP/2
    JavaScript IOT (Node.js, IoT.js)

    Network Layer Protocols

    The network layer is an infrastructure layer within IoT reference architectures, and handles the addressing and routing of data packets. IPv6 is an anew standard that exceeds IPv4 in the total number of address spaces available.

    6LoWPAN *IPv6 over Low-Power Wireless Personal Area Networks
    6TiSCH *IPv6 over the TSCH Mode of IEEE 802.15.4e
    6Lo *IPv6 over Networks of Resource-constrained Nodes
    IPv6 over Bluetooth Low Energy
    IPv6 over G.9959

    IoT Wireless Standards

    Wireless standards are the technologies that bridge wired connections/hardware through wireless transmission and reception medium. Similar to how Ethernet, Fiber-optic, USB, HDMI, and etc. are used for wired connections, there are a variety of wireless protocols designed to serve within a range of application requirements (industrial monitoring, smart-home networks, offshore sportsbooks, connected vehicles, and many others). Typically, these protocols can be broken into three categories; Medium/Short Range Wireless Standards that serve peer-to-peer (P2P), LAN, PAN, and HAN connectivity; Cellular and Mobile Wireless Standards that are generally WAN based standards that use the cellular network; and most recently, Low-Power Wide Area Network (LPWAN) standards that are designed to offer extremely wide coverage using low power and low data rate protocols.

    Medium/Short Range IoT Wireless Standards (P2P, LAN, PAN, HAN)

    Zigbee/IEEE 802.15.4
    Thread
    Weave
    Bluetooth
    Z-Wave
    WiFi
    WirelessHART
    RFID/NFC
    DASH7
    EnOcean *Energy Harvesting
    DiGiMesh
    MiWi

    Cellular and Mobile Wireless Standards (WAN)

    3G
    4G LTE
    4G LTE-A
    4G LTE Pro
    4G+
    5G Sub-1 GHz Low-Band
    5G Sub-6 GHz Mid-Band
    5G Millimeter-wave High-Band
    LTE-M *Cellular for Machines
    EC-GSM *Extended Range GSM also EC-GSM-IoT

    Low-Power Wide Area Network (LPWAN) Wireless Standards/Protocols

    Long-Range (LoRa)
    SigFox
    Ingenu
    Weightless
    NB-IoT *Narrow Band IoT
    NWave
    RPMA

    Though wireless technologies do use RF frequencies to send and receive information (wireless connection), they do require several critical physical RF signal chain components to do so. These components include antenna, RF transmission lines (coax and microstrip), baluns, resistors, capacitors, inductors, attenuators, low noise amplifiers (LNA), power amplifiers (PA), mixers, isolators, amongst a wide variety of testing instruments and components.

    References

    1. https://www.pasternack.com/blog/uncategorized/iot-wireless-standards-in-a-nutshell/