Difference Between Coplanar Waveguide, Microstrip, Stripline, & Other Planar Transmission Lines

  • Categories

  • Archive

  • Planar transmission lines are used to carry a variety of analog, RF, and digital signals on insulative, planar substrates from kilohertz to hundreds of gigahertz frequencies. Planar transmission lines are constructed of one or more layers of metal traces with one or more parallel metal traces. There are several common types of planar transmission lines: stripline, suspended stripline, microstrip, coplanar waveguide, slotline, and imageline, of which there are also variants. Each type of planar transmission line exhibits different dominant transmission modes, max frequency, characteristic impedance range, and unloaded Q factor.

    Key Takeaways 

    • • Planar transmission lines (microstrip, stripline, coplanar waveguide (CPW), slotline) each have distinct structures, field distributions, fabrication demands, and performance trade-offs.  
    • • Stripline: signal trace is sandwiched between two ground planes, giving excellent shielding and low radiation, supporting true TEM mode. 
    • • Microstrip: signal trace on top of a dielectric substrate with a ground plane beneath – easier to fabricate, but more radiation loss and quasi-TEM propagation.  
    • • Coplanar Waveguide (CPW): signal trace and adjacent ground planes on the same substrate surface (coplanar), good for transitions, narrow traces, and certain high-frequency layouts.  
    • • Performance criteria differ e.g.; typical maximum useful frequency, characteristic impedance range, and unloaded Q factor vary between line types.  
    • • Choosing the right line type depends on application constraints: fabrication complexity, layer stack-up, shielding needs, frequency band, loss budget, and cost.
    •  

    Types of Planar Transmission Lines

    • Stripline: A “strip” conductor embedded within a dielectric substrate and sandwiched between two ground plans
    • Suspended Stripline: A stripline that is suspended in air between the ground plans, with the air gaps being above and below the strip.
    • Microstrip: A strip conductor on top of a dielectric substrate with a ground plane beneath the substrate.
    • Coplanar Waveguide: a strip conductor with two ground planes parallel and on either side of the strip on the same dielectric substrate.
    • Slotline: a slot separating two metal traces on the same plane of the dielectric substrate.
    • Finline: A slotline that is rotated +/- 90 degrees inserted into the E-plane of a rectangular metal waveguide.
    • Imageline: A dielectric slab waveguide with a strip of dielectric on a metallized plane.

    Typically the outer, top, or bottom traces of a planar transmission line are grounded with the interior trace as the signal traces. These physical structures allow for the development of transmission line modes, namely transverse electromagnetic (TEM), transverse electric (TE), transverse magnetic (TM), quasi-TEM, longitudinal-section electric (LSE), and longitudinal-section magnetic (LSM), depending on the planar transmission line configuration. The electrical behavior of a planar transmission line depends on how the field lines are distributed through air and the substrate (dielectrics) and how the field lines are coupled to the signal and ground traces or metalization.

    Dominant Modes Of Planar Transmission Lines

    • Stripline: TEM
    • Suspended Stripline: TEM, quasi-TEM
    • Microstrip: Quasi-TEM
    • Coplanar Waveguide: Quasi-TEM
    • Slotline: Quasi-TE
    • Finline: LSE, LSM
    • Imageline: TE, TM

    Max Frequency (Typical)

    • Stripline: 60 GHz
    • Suspended Stripline: 220 GHz
    • Microstrip: 110 GHz
    • Coplanar Waveguide: 110 GHz
    • Slotline: 110 GHz
    • Finline: 220 GHz
    • Imageline: >100 GHz

    Characteristic Impedance Range (with substrate relative permittivity of 10)

    • Stripline: 30 – 225 Ohm
    • Suspended Stripline: 40 – 150 Ohm
    • Microstrip: 10 – 110 Ohm
    • Coplanar Waveguide: 40 – 110 Ohm
    • Slotline: 35 – 250 Ohm
    • Finline: 10 – 400 Ohm
    • Imageline: ~26 Ohm

    Unloaded Q Factor (with substrate relative permittivity of 10)

    • Stripline: ~400
    • Suspended Stripline: 600 @ 30 GHz
    • Microstrip: 250 @ 30 GHz
    • Coplanar Waveguide: 300 @ 30 GHz
    • Slotline: 200 @ 30 GHz
    • Finline: 550 @ 30 GHz
    • Imageline: 2500 @ 30 GHz

    Planar transmission lines with “loose” field lines may also couple with nearby metallization on a substrate or any metallic housing or structures within close proximity. This can result in planar transmission lines exhibiting additional and undesirable spurious modes. Hence, there are planar transmission line types and variants that use tightly coupled grounded structures nearby, or even completely surrounding, the signal traces. Though these tightly coupled transmission lines tend to exhibit higher conductor losses, they exhibit lower radiation losses, better spurious mode suppression, and possibly higher frequency performance. The trade-off in greater grounding/shielding is the additional cost, weight, and a possible increase of performance sensitivity to substrate and metalization fabrication tolerances.

    There are also varying complexities associated with fabricating each transmission line type and their variants. For instance, planar transmission lines with only surface traces on a single layer, such as standard coplanar waveguides or slotlines may be lower cost and more easily manufactured than microstriplines that require two layers of metal or grounded coplanar waveguides with metallized vias connecting the surface ground traces to the bottom ground layer.

    Common Stripline Variants

    • Suspended Stripline
    • Bilateral Suspended Stripline
    • Two Conductor Stripline

    Common Microstrip Variants

    • Suspended Microstrip
    • Inverted Microstrip
    • In-box Microstrip
    • Trapped Inverted Microstrip

    Common Coplanar Waveguide Variants

    • Grounded Bottom or Common Bottom Coplanar Waveguide (GBCPW or CBCWG)
    • Grounded Coplanar Waveguide (GCPW)
    • Coplanar Strips
    • Embedded Coplanar Strips

    Common Slotline Variants

    • Antipodal
    • Bilateral

    Common Finline Variants

    • Unilateral
    • Bilateral
    • Antipodal
    • Strongly Coupled Antipodal
    • Insulated

    Resources
    Jarry, Pierre; Beneat, Jacques, Design and Realizations of Miniaturized Fractal Microwave and RF Filters, Wiley, 2009 ISBN 0-470-48781-X.
    Edwards, Terry; Steer, Michael, Foundations for Microstrip Circuit Design, Wiley, 2016 ISBN 1-118-93619-1
    Wanhammar, Lars, Analog Filters using MATLAB, Springer, 2009 ISBN 0-387-92767-0
    Rogers, John W M; Plett, Calvin, Radio Frequency Integrated Circuit Design, Artech House, 2010 ISBN 1-60783-980-6
    Maloratsky, Leo, Passive RF and Microwave Integrated Circuits, Elsevier, 2003 ISBN 0-08-049205-3

    FAQs (Frequently Asked Questions) 

    Q1. What is the role of the dielectric material in these transmission lines? 

    A: The dielectric material (such as Rogers, FR-4, or PTFE) defines the effective permittivity and loss of tangent, which influences signal velocity, attenuation, and impedance. A high-quality, low-loss dielectric ensures better performance at microwave and millimeter-wave frequencies. 

    Q2. What does “quasi-TEM” mode mean in microstrip and CPW lines? 

    A: A quasi-TEM (quasi-Transverse Electromagnetic) mode means that electric and magnetic fields are mostly perpendicular but not perfectly so, because part of the field exists in air and part within the substrate. This slightly distorts the field and causes frequency-dependent impedance. 

    Q3. Why is impedance control important in planar transmission lines? 

    A: Maintaining a consistent characteristic impedance (usually 50 Ω) ensures minimal reflection, optimal power transfer, and low return loss. Variations in substrate height, dielectric constant, or trace width can affect impedance and overall signal integrity.