Pasternack Blog

  • Categories

  • Archive

  • Constraints and Considerations for Bi-directional Amplifiers

    08/31/2017

    Bi-directional amplifiers are used to strengthen communication signals between two points for a wide array of applications. This include boosting signals along large subterranean or in-building distributed antenna systems (DAS), acting as a repeater to a remote observation station, and even enabling rapidly deployable portable networks with unmanned aerial vehicles (UAVs). As many modern uses ..

    Read Full Article

    Introduction to RF Baluns

    08/17/2017

    A balun, meaning balanced-unbalanced, is a three-port device that converts differential signals to single-ended signals, and vice versa. Hence, a balun presents a 180° phase shift between the signals in the balanced end, unlike a power divider with no phase shift between the splitting ports. This functionality allows for baluns to take the input, or ..

    Read Full Article

    Phase Noise and Additive Phase Noise Limit Radar and Communications System Performance

    05/25/2017

    Phase noise and its time-domain counterpart, jitter have been studied in radar and communications systems since the phenomenon was first observed. Though always a concern, recent advances in high-speed digital modulation schemes and advanced radar, which also used complex digital modulation techniques for pulse compression, have led to radar and communication systems being more susceptible ..

    Read Full Article

    The Difference between MIL-STD, MIL-HDBK, MIL-DTL, MIL-PRF and MIL-SPEC

    05/18/2017

    The US defense standards, commonly referred to as MilSpec, are developed by the US DoD for the purpose of enhancing interoperability among critical defense systems. The goal of the standards is to provide precise descriptions on the procedures and practices for the design, manufacturing, and deployment of military devices and equipment. Ultimately, the standards aim ..

    Read Full Article

    What is Passive Intermodulation (PIM) Distortion, and how can it be Mitigated?

    04/27/2017

    Passive intermodulation (PIM) distortion is a wireless communication system degrading phenomenon that has been a concern for cellular telecommunications, satellite communications, and wireless network development. PIM is such a concern in cellular/wireless communications that there are entire distinct Low PIM Components and Cable Assemblies product lines designed to aid in preventing or mitigating PIM distortion. ..

    Read Full Article

    What do RoHS, REACH, and WEEE Mean for RF/Microwave Components, Manufacturers and Assemblers?

    04/13/2017

    RoHS, also known as Lead-Free, stands for Restriction of Hazardous Substances. RoHS originated in the European Union and restricts the use of six hazardous materials found in electrical and electronic products. All applicable products in the EU market after July 1, 2006 must pass RoHS compliance. The substances banned under RoHS are lead (Pb), mercury ..

    Read Full Article

    Practical Mixers 101

    03/23/2017

    Introduction to Mixers A microwave frequency mixer is a 3-port electronic circuit that combines two or more signals into one or two composite output signals, and are categorized as switching mixers or nonlinear mixers– although many mixers are configured with both. Using diodes, the mixer is passive and has a conversion loss. Using active devices, ..

    Read Full Article

    All About Jitter

    01/26/2017

    Though a detailed explanation of jitter can be highly complex mathematically, simply put, jitter is the deviation of a signal from its ideal periodic behavior in terms of frequency, signal amplitude, or phase. There are many contributors to jitter in a signal, from the source itself to outside interferers. Additionally, jitter can be described similarly ..

    Read Full Article

    IMS 2015 Video of Our Announcement About the All New RF Cable Assembly Creator

    06/01/2015

    International Microwave Symposium 2015 (IMS 2015) tradeshow conference / symposium and expo video of Pasternack demonstrating our new Cable Creator for RF cable assemblies. The video from the IEEE IMS 2015 conference, trade show and expo in Phoenix, AZ shows the Pasternack booth while the new RF cable assembly tool, the Cable Creator, is demonstrated ..

    Read Full Article

    Japanese RF, Microwave and Millimeter Wave Components Website Launched by Pasternack

    05/15/2015

    Japanese RF, microwave and millimeter wave website www.pasternack.jp, recently launched by Pasternack, has greatly expanded reach into the Japanese market. Our Japanese RF components website is translated by radio frequency industry experts into local language and offers local Japan eCommerce options, previously not available from the company’s USA website, Pasternack.com. This RF/microwave website in Japanese ..

    Read Full Article
    Jump to of 9