Pasternack Blog

  • Categories

  • Archive

  • How to Find Frequency from Wavelength: A Step-by-Step Guide

    02/09/2023

    In the world of electromagnetic waves and wireless communication, understanding the relationship between frequency and wavelength is crucial. Whether you’re working with radio frequencies, microwaves, or optical signals, knowing how to find frequency from wavelength can help you design and troubleshoot wireless systems, antennas, and transmission lines. The math here quietly powers a surprising amount ..

    Read Full Article

    What are the common very high frequency/ultra-high frequency (VHF/UHF) [30 MHz to 300 MHz, and 300 MHz to 1000 MHz] antenna types?

    02/02/2023

    VHF/UHF stands for very high frequency and ultra-high frequency, respectively. These frequency designations are in both the ITU and IEEE radar bands, but in this case we are discussing IEEE radar bands VHF and UHF, 30 MHz to 300 MHz and 300 MHz to 1000 MHz in the US. This is an important note, as ..

    Read Full Article

    What is a Waveguide Magic Tee?

    01/19/2023

    A Waveguide Magic Tee is a 180-degree hybrid power divider with 4 ports made from a single waveguide structure. The Magic Tee has been around for over 70 years and was a product of development during World-War II. The structure of a Magic Tee is a combination of an E-plane waveguide arm meeting a H-plane ..

    Read Full Article

    SMA Connector Overview

    12/29/2022

    SMA Coaxial Connectors, or just SMAs, are one of the most common coaxial connector types used throughout the RF, microwave, and even millimeter-wave (mmW) industries. SMA stands for subminiature version A and was developed in the 1960s. The interface dimensions and other aspects of the SMA connector are detailed in MIL-STD-348 and was originally designed ..

    Read Full Article

    Coaxial Cable Assemblies for Rugged Outdoor Applications

    12/15/2022

    RF Coaxial Cable Assemblies are used in virtually all environments where wireless systems are deployed. Coaxial cable assemblies are integral internal parts of many wireless systems, and they are also used as interconnects between systems. These cable assemblies are often anywhere from a few inches long to hundreds of feet in length. This range of ..

    Read Full Article

    Power Added Efficiency (PAE) Calculator Explained

    12/01/2022

    RF power amplifiers typically have an input, output, and power supply rails. These rails can be either positive, negative, or dual positive and negative voltages. The input, output, and power supply rails all have recommended operating ranges of power, voltage, and current. This range is specified to nominal operation in what the manufacturer was able, ..

    Read Full Article

    Pasternack’s 50th Anniversary! An Interview with the Man who Started it all

    11/14/2022

    Pasternack has a milestone anniversary this year! Fifty years later, Pasternack products are as relevant and renowned as ever, and there’s no slowing down. To celebrate this momentous occasion, we recently had the opportunity take a trip down memory lane and learn the history of the brand from Murray Pasternack, the founder of Pasternack. Read ..

    Read Full Article

    Coaxial Cable Impedance Calculator

    11/03/2022

    The dominant use of coaxial cable in RF & Microwave applications is as a transmission line. Coaxial cables are extremely useful transmission lines as the coaxial nature of the transmission line provides relatively efficient transmission from DC to a cut-off frequency, which is a function of the geometries of the coaxial components of the cable. ..

    Read Full Article

    Antenna Downtilt & Coverage Calculator Chart

    10/20/2022

    An Antenna Downtilt and Coverage Calculator, or Antenna Tilt Calculator, aids the user by providing an approximate downward angle at which to install a directional antenna to reach desired signal strength and coverage between a transmitter and receiver at different heights and some distance away. An example use case is when a cell-tower directional transceiver ..

    Read Full Article

    VSWR, Return Loss, Insertion/Transmission loss vs. Transmission Power

    09/22/2022

    In an ideal RF system, all of the energy from the RF source is transferred to the load. An example of this would be a transmitter delivering a signal to an antenna with the interconnect between the two signal chain components operating at 100% efficiency. Clearly, this isn’t the case, and factors like impedance mismatch ..

    Read Full Article
    Jump to of 38