Pasternack Blog

  • Categories

  • Archive

  • New Applications for Bi-Directional Amplifiers – Unmanned Systems

    01/07/2021

    In a similar way to how wireless technology is enabling new functionality and opportunities in civilian life, there are a wealth of military applications embracing, and being enhanced, by wireless technology. Unlike civilians, military operators require a much higher level of reliability and redundancy, as a few second gap in coverage for a military operator ..

    Read Full Article

    Signal Chain Discussion Series: Local Oscillators

    12/17/2020

    A local oscillator (LO) is an electronic oscillator that generates a very narrow bandwidth signal, or tone, with high purity and stability for use in frequency conversion circuits and timing. As the performance of frequency conversion circuits and timing systems are often dependent on the LO performance, the quality of the oscillator and LO electronic ..

    Read Full Article

    Signal Chain Discussion Series: Difference Between IF & RF

    12/10/2020

    In many cases in RF/Microwave electronics it is advantageous to generate, modulate, receive, and demodulate communication and sensing signals at frequencies lower than the RF transmission/reception carrier frequency. The frequency difference between the modulation/demodulation (baseband) signals and the RF signals may be so vast, that multiple frequency conversion stages may be required. In these instances, ..

    Read Full Article

    Signal Chain Discussion Series: Circulators & Isolators Versus Switches As Duplexers

    12/03/2020

    Circulators/isolators and switches are both commonly used in the RF front-end of communication and radar systems. The purpose of circulators/isolators and switches in RF front-ends is to enable the use of transmission and reception from the same antenna, duplexing. For instance, in a transmit/receive module (TRM) for an active antenna system (AAS) (phased array antenna), ..

    Read Full Article

    Signal Chain Discussion Series: Transmit/Receive Module

    11/12/2020

    Though transmit/receive modules (TRMs) have been used for some time in active electronically scanned array (AESA) radar technology, the benefits of phased array antenna and multi-input-multi-output (MIMO) for 5G applications have brought this technology to the mainstream. Given that phase array antennas for millimeter-wave 5G may employ up to, and possibly beyond, 64 antennas elements ..

    Read Full Article

    RF Oscillator Features and Performance Considerations For 5G Applications

    11/05/2020

    Given the stringent timing requirements of 5G network and wireless applications, RF oscillator performance is of increasingly critical importance. Noise and phase noise are among the most significant of these requirements, as these parameters have the greatest impact on communication signal quality and receiver capability. Though noise and phase noise have always been RF oscillator ..

    Read Full Article

    Signal Chain Discussion Series: Communications Transceiver

    10/29/2020

    A communications transceiver performs the task of converting digital or analog signals to RF, transmitting those signals, and receiving incoming signals for conversion back to digital or analog signals. Hence, the key components of a communications transceiver are the modulation/demodulation circuitry, transmitter, and receiver. Depending on the architecture of the communications transceivers, direct digital synthesizers ..

    Read Full Article

    Highlights of Low Noise Amplifier Input-Protection

    10/22/2020

    Though highly sensitive receivers require low noise amplifiers (LNAs) that are also sensitive to extremely weak signals, this sensitivity can also put the receiver front end LNAs at risk of desensitization, latent performance degradation, or destruction. In the presence of a signal strength at the input of an LNA that exceeds the input signal power ..

    Read Full Article

    Basics of Coaxial Connector Attachment

    10/15/2020

    Coaxial assemblies are nearly ubiquitous for RF/microwave applications, with the exception of applications that require waveguide or planar transmission lines for efficiently conducting RF signals between components and devices. Hence, coaxial assemblies are found in use cases including within an assembly, bench-top instrument/device, indoor, outdoor, in aircraft, land-mobile vehicles, machinery, robotics, spacecraft, satellites, and more. ..

    Read Full Article

    Understanding SMA RF Cables: What They Are and How They’re Used

    10/14/2020

    In many high-frequency applications, SMA RF cables are essential for transmitting reliable signals. Known for their small size and high performance, SMA RF cables are widely used in industries such as telecommunications, aerospace, and defense. With a standard 50-ohm impedance, these cables ensure excellent signal integrity, making them an indispensable solution for various RF applications. ..

    Read Full Article
    Jump to of 38