Labor Day Closure: We’ll be closed Monday, Sept. 7, and reopen Tuesday, Sept. 8.
Tee (T) attenuator calculator from Pasternack allows you to determine theresistor values (R1 & R2) for a the RF component. The tee (T) attenuator (pad) formula in the calculation for resistor values is measured in Ohms. The Tee attenuator (T-pad) is a specific type of attenuator circuit which resembles the shape of the letter "T". The Tee attenuator consists of one series resistor at the input and two parallel, one of which is grounded while the other goes to output.
Visit Pasternack's RF coaxial attenuators page for product details.
**Note: Like our tee (T) attenuator calculator, all of our RF calculators allow SI prefixinput. For example, if you wish to input "25000000", just type "25M" instead. See the quick-reference tablebelow for all compatible SI prefixes.