Labor Day Closure: We’ll be closed Monday, Sept. 7, and reopen Tuesday, Sept. 8.
Pasternack's Stripline Impedance Calculator uses the dimensions of the stripline, as well as the dielectric constant, to compute the characteristic impedance.
Note: Units for width and height must be consistent
A stripline consists of a central conductor surrounded by dielectric material between two groundplanes. Striplines, in many cases, can be used where microstrips would be, so long as size is not a constraint. In fact, striplines often make components such as band-pass filter's more accurately, with more symmetric roll-off and no lower cutoff frequency.
**Note: Like our stripline impedance calculator, all of our RF calculators allow SI prefix input. For example, if you wish to input "25000000", just type "25M" instead. See the quick-reference table below for all compatible SI prefixes.